Technical FAQs

Ask a Question

What is the default IP Address of the Modicon M258 controlller.

When Modicon M258 controller is  straight out of the packaging box, the default IP address is

10.10.x.y (Where x and y are the last two places from the MAC Address but in "Decimal").

Was this helpful?
What can we do to improve the information ?