Technical FAQs

Ask a Question

Is it possible to change the device type of controller or Human Machine Interface(HMI)controller, once project is created in SoMachine.

In current SoMachine version ( V2.0 ) there is no option to change device type of controller or Human Machine Interface(HMI)controller,once project is created in SoMachine.

Alternatively,in future version of SoMachine greater than V3.0, there shall be a function "Update family" available to do so.
 
What you can do to change a HMI or the HMI controller :
  1. Export VJD(VijeoDesigner) project.
  2. Open in VJD standalone.
  3. Change HMI type as desired.
  4. Export VJD project file and then import in SoMachine project.
 
Was this helpful?
What can we do to improve the information ?