Technical FAQs

Ask a Question

What would be the maximum timer preset value in Quantum.

The maximum timer preset value is 4294967.295 seconds
Was this helpful?
What can we do to improve the information ?