Technical FAQs

Ask a Question

Is it possible to display actual machine shaft RPM on the ATV71 graphic display.

It is possible if ATV71 is used in open loop, an optional encoder board can be used to read the encoder signals mounted on the shaft.
Then customize the monitoring parameter MMF ("Measured Speed") to convert Hz into machine shaft RPMs.
 
Note- Parameters customization can be accessed in "Expert" access level only.
Was this helpful?
What can we do to improve the information ?