Technical FAQs

Ask a Question

What are the faults that can be reset with the automatic restart function, after the cause has disappeared on Altivar 71 and Altivar 61 drives.

Refer the attached list of the faults which can be reset with the automatic restart function.
Was this helpful?
What can we do to improve the information ?