Technical FAQs

Ask a Question

Is torque limit function (tLI) effect all the duration when motor is powered in Altistart 48.

The "tLI" function is enabled only in acceleration and deceleration state.
Was this helpful?
What can we do to improve the information ?