Technical FAQs

Ask a Question

Is it possible to use the braking module VW3A11701 of the Altivar 11 on the Altivar 12 drive.

The braking module VW3A11701 of Altivar 11 can used on the Altivar 12 and vice versa, the braking module
VW3A7005 of
Altivar 12 can use on Altivar 11.
Was this helpful?
What can we do to improve the information ?