Technical FAQs

Ask a Question

What is the meaning of the message "Circuit Trip" on a Sepam 40 series relay.

The ‘Circuit Trip’ is related to the Circuit Breaker control features.
It indicates that the Input I11 or input I12 on Sepam is not receiving a signal. If you are not using a Circuit Breaker control the recommendation is not to use this function.
Was this helpful?
What can we do to improve the information ?