Technical FAQs

Ask a Question

How to troubleshoot the communication issues between Laptop and Programmable logic controller(Twido/TSX Micro/Premium) using TSXCUSB485 cable.

It is possible to use TSXCUSB485 + TSXCRJMD25 Programming cable to upload application program from programmable logic controller (PLC) to
Laptop/Computer and download from Laptop to PLC(like Twido,TSX Micro and Premium.The important  point is to troubleshoot the communication
between Laptop/computer (installed with Driver Pack V2.5/V2.6)and controller  and details of the troubleshoot procedure is explained in attached file.
Was this helpful?
What can we do to improve the information ?