Technical FAQs

Ask a Question

How to establish communication between XBTN401 Human Machine Interface(HMI)and Zelio Logic through Zelio protocol.

It is possible to establish communication between XBTN401 Human Machine Interface(HMI)and Zelio Logic through Zelio protocol using 
SLIN and SLOUT function.
Refer to attached file for technical resolution for the procedure including sample programs.
Was this helpful?
What can we do to improve the information ?