Technical FAQs

Ask a Question

Why even after the registration key validation; every time while launching the software, a small window is appearing and asking for the registration.





User can just click "OK" and go for the next screen to work on My Ecodial L.(if the software evaluation period is
over; then the OK button will be disabled; user has to follow the registration steps once again; or he can use his
registration key to activate the software).
 
This window, appearing even after the registration key validation is considered as a functional Error. But since
Jan” 2010, the development of My Ecodial L has been stopped. So, the bug is not fixed.
Was this helpful?
What can we do to improve the information ?