Technical FAQs

Ask a Question

What is the minimum motor current to be used with Altistart 22 Soft Starter.

The minimum motor current value should be 0.4 ICL (nominal Soft Starter current). So, the connected motor current
shall not be less then this value to make sure the motor is working well.
Was this helpful?
What can we do to improve the information ?