Technical FAQs

Ask a Question

Can you provide sample examples for Peer to Peer communication between two numbers of Twido Controllers TWDLCAE40DRF.

Refer to attached sample projects for Peer to Peer communication between two numbers of Compact Twido Controllers
TWDLCAE40DRF using the inbuilt Ethernet RJ-45 Ports of the respective controller along with possible system architecture.
Was this helpful?
What can we do to improve the information ?