Technical FAQs

Ask a Question

How to establish Remote Link between Twido Controllers and what is the maximum allowed number of slaves.

The remote link is possible only with one port(Port1 or 2)of Twido,but it’s possible to mix remote I/O and Peer controller.

For Remote Link(Remote I/O): The exchanges are automatic between a twido master and Twido 
slaves(7 maximum without application).Exchanges are available only with bases(No expansion).

For Remote Link( Peer Controller):The exchanges are automatic between a twido master and Twido 
slaves (7 maximum )with a table (4 words maximum).
 
Refer to attached resolution for illustration of Remote link communication with an example to read the input %I0.1
of the master N°0 and write the value in the output %Q0.2 of a slave N°4.
Was this helpful?
What can we do to improve the information ?