Technical FAQs

Ask a Question

Provide the communication port details of Twido Controllers.

All Twido Controllers have inbuilt 8-pin MiniDIN RS485 Port1 and other optional Port2 based on part numbers
have to ordered separately and refer to attached file for pin description of the communication ports.
Was this helpful?
What can we do to improve the information ?