Technical FAQs

Ask a Question

Is it possible to use several TEXT function block in ZelioSoft.

Yes, it is several TEXT  function block in FBD using a CAM block function. Refer to attached program example realized in
ZelioSoft2V4.4 and it is possible to change of Text Block using Z button.
Was this helpful?
What can we do to improve the information ?