Technical FAQs

Ask a Question

Is it possible to install the C60 range MCB up side down.

C60 range of MCBs can be mounted in any position without deterioration of their characteristics. So it is possible
to install the C60 MCB up side down.
Was this helpful?
What can we do to improve the information ?