Technical FAQs

Ask a Question

What is the dielectric test value for the DC voltage of the C60 PV DC ranges MCB.

According to the standard IEC 60947-2, the dielectric test value for the DC voltage is 1415 V.
Was this helpful?
What can we do to improve the information ?