Technical FAQs

Ask a Question

What is the maximum number of add-on modules that can be fitted on the V5 (125A) and V6 (175A) vario switch body.

The maximum no of add on module is 2 for V5 & V6 switch bodies. One module can be connected
on each side of the switch body.
Was this helpful?
What can we do to improve the information ?