Technical FAQs

Ask a Question

Is it possible to clear the Fault History in Altivar 61/71.

It is not possible to reset fault history except changing control block.
The mechanism of the fault history is the drive save 8 last faults stored in the fault history menu (In 1.10 DIAGNOSTICS menu ) ,
then if a new fault appears, the old one will be removed in the list of fault history and it will be placed by the new one.
Was this helpful?
What can we do to improve the information ?