Technical FAQs

Ask a Question

Can you give any example of Modicon M238 Communication with ATV31 on Canopen using NMT function block.

Refer to  attachment folder a POU to program the NMT function block (Stop/Start Canopen Device) and the
REC_EMCY_DEV which return the last emergency received from the device ATV31.
Was this helpful?
What can we do to improve the information ?