Technical FAQs

Ask a Question

What modbus function codes are supported by Modicon M238 Controller.

Refer to attached file for Modbus function codes supported by M238 Controller as modbus slave.

1.Out of %MW register access possible to read and write
for bit access only read access is available,but the bit element is an extract of %MW.
All M238 Controller bit %MX0.0 to MX0.7 + %MX1.0 to MX1.7 are member of the register %MW0 .
2.No direct access to %MB,where %MW0 include %MB0+%MB1.
3.For Bit access for bit access read,the rule is same for read %I function request 2 and %Q function request1.
4.To acces to a bit number n between 0 and 7 of mapped object byte I_QX.i.n of M238 Controller
For First byte,number is n
For second byte,number is n+8
For third byte,number is n+16
For byte number I,number is n+ (i)*8
For number 15,this is the High upper bit located in the secoond byte  is %Ix1.7.
Was this helpful?
What can we do to improve the information ?