Technical FAQs

Ask a Question

What is the maximum number of characters that can be send with the function send SMS.

It is possible to send 160 characters per SMS.
1120bit coded with 7bit ASCII ( No special characters ).
 
Thus,if user uses the standard character table(7bit coded),he can send 160 characters with SoMachine V3.0.
Was this helpful?
What can we do to improve the information ?