Technical FAQs

Ask a Question

How to use HSCMAIN and HSCGETCAPTUREDVALUE function blocks in SoMachine using M238 Controller.

Refer to attached SoMachine example to set up a Main counter for M238 Controller using HSCMAIN and HSCGETCAPTUREDVALUE function blocks.
The input0(%I0) is the pulse signal and the input 3 (%I3) is used to capture the current value of the counter on the falling edge.
The "front" input is used to preset the counter.
Was this helpful?
What can we do to improve the information ?