Technical FAQs

Ask a Question

How to update Modicon M238 Controller RTC( Real Time Clock) via XBTGT series terminals.

Refer to attached file for an application project which uses the Modbus protocol for updating Modicon M238
Controller (TM238LFDC24DT)
Real Time Clock via XBTGT terminals (Example with XBTGT2390).
Was this helpful?
What can we do to improve the information ?