Technical FAQs

Ask a Question

Why the parameter setting is disappeared automatically, when the power off and on of Altivar 21 drive (with Lonwork card).

According to the LonWorks documentation, the LonWorks card overrides automatically some drive parameters.

Refer to attached file.
If you modify these parameter by HMI local, at each Power on, the LonWorks card will
override the value.
It means that theses parameter have to be write only by LonWorks, even if the card is only used in monitoring.
Was this helpful?
What can we do to improve the information ?