Technical FAQs

Ask a Question

How to Display Time and Date of the Zelio Logic into Magelis XBTN401 using Zelio Protocol.

Refer to attached sample programs which uses Archive Function and it enables to read the current time (without second) and
subsequently,user can transfer the output in the SLOUT function.
Was this helpful?
What can we do to improve the information ?