Technical FAQs

Ask a Question

How to use PRESET H-METER(Preset Hour Counter)Function Block in Zelio Logic.

PRESET H-METER (Preset Hour Counter)Function Block(FB) will active a output of FB when the first input of FB is at TRUE during
a delay determine by configuration. The accuracy of PRESET H-METER Function Block in FBD (Function Block Diagram)
is 1second + 2 Time cycle.
Refer to attached sample program using PRESET H-METER Function Block in FBD Mode.
Was this helpful?
What can we do to improve the information ?