Technical FAQs

Ask a Question

What are the switching time for the static and relay outputs of Zelio Logic.

The reponse time for Static output Zelio Logic is <=1 ms (Maximum value is 1ms) irrespective of the change
level ( 0 to 1 or 1 to 0 )operation.
The reponse time for Relay ouputs is 10 ms when user have to set the output
and 5 ms when user have to reset the output.
Was this helpful?
What can we do to improve the information ?