Technical FAQs

Ask a Question

ELF 3234 Meter is not displaying power factor after power ON.

By Default, ELF3234 meter comes with Power setting (watt), Power Factor is a user selectable,
so you need to select power factor in  -->
RMS -->Power Factor.
Was this helpful?
What can we do to improve the information ?