Technical FAQs

Ask a Question

ELF 3234-3 Meter is displaying power factor (PF) and watt (W) but not displaying VA/VAR.

By Default, ELF3234-3 meter comes with Power Factor setting ( PF ),you can select any one from W/VA/VAR, which
are user selectable parameters. It is possible to select only one parameter from W/VA/VAR.
Was this helpful?
What can we do to improve the information ?