Technical FAQs

Ask a Question

What are all options available in the EM3460 Time of use (TOU) feature.

Below options are available in the EM3460 Time of use (TOU) feature
 
1.    In a year, maximum six seasons and 10 public holidays.
2.    In a season, maximum three weekends, rest as week days.
3.    In a day, maximum eight tariff timings and eight sub-integrators.
4.    Separate MD registers for different time slots and also separate demand UL and LL for the different time slots.
Was this helpful?
What can we do to improve the information ?