Technical FAQs

Ask a Question

What is the operating time to take into account the RUN/STOP order via Logic input in Altivar 32.

Operating time to take into account the RUN order via Logic input in Altivar 32 is 8ms +/- 1ms and Operating
time to take into account the STOP order via Logic input is 6ms +/- 1ms.
Was this helpful?
What can we do to improve the information ?