Technical FAQs

Ask a Question

What is the operating time to take into account the RUN/STOP order via Logic input in Altivar 71/61.

Operating time to take into account the RUN order via Logic input in Altivar 71/61 is 2ms +/- 1ms and Operating
time to take into account the STOP order via Logic input is 2ms +/- 1ms.
 
Was this helpful?
What can we do to improve the information ?