Technical FAQs

Ask a Question

Is it possible to replace the Telemecanique logo by a specific one in Graphic display terminal (Keypad) of Altivar 71/61.

Yes, it is possible to replace the Telemecanique logo by a specific one in Graphic display terminal
of Altivar 71/61.
The software is the "Keypad Flash tool" available with the Schneider with the
reference VW3A9702.
Was this helpful?
What can we do to improve the information ?