Technical FAQs

Ask a Question

Which operating systems were supported by Vijeo Historian 4.3.

Following Operating Systems were supported by Historian 4.3 :
Windows XP Business SP3
Windows Vista Business (or higher) SP2
Windows Server 2003 SP2
Windows Server 2003 R2
Windows 7 SP1
Windows Server 2008 R2
Note : Vijeo Historian runs in 32 bit mode on a 64 bit operating system.
Was this helpful?
What can we do to improve the information ?