Technical FAQs

Ask a Question

How to set screen update time in Vijeo Citect projects.

To set the screen update time you have to set the [Page]ScanTime form 1 to 60000 (milliseconds).
It`s default value is 250.The Page ScanTime determines how often (in milliseconds) the Animator
refreshes a graphics page at runtime.
A value of 250 indicates that it refresh the page 4 times per second.  
This parameter is modified by the Computer Setup Wizard as well as the Computer Setup Editor.
Any value you enter into your project parameters will be overridden by that specified in the Wizard.
Was this helpful?
What can we do to improve the information ?