Technical FAQs

Ask a Question

Is the Harmony XB5S Biometric Switch UL listed.

Yes, the Harmony  XB5S Biometric switches is UL508 certified. It is also CE marked and has CSA certifications
 for Canada and USA (to UL508 requirements).
Was this helpful?
What can we do to improve the information ?