Technical FAQs

Ask a Question

What is the maximum number of fingerprints the Harmony XB5S Biometric Switch can hold.

The Harmony XB5S Biometric switches can remember up to 200 fingerprints including different
fingerprints from the same operator or administrator.
Was this helpful?
What can we do to improve the information ?