Technical FAQs

Ask a Question

What is the replacement of GSKC24VACDC.

Emergency Stop function Preventa Safety module reference GSKC24VACDC  with 3 N/O S Safety Circuit
Outputs has been discontinued.Old reference GSKC24VACDC can be replaced by New Reference
XPSAK311144 Or XPS AF5130 based on customer application.
 
XPSAK311144 – Preventa Safety Module For Emergency stop, switch, sensing mat/edges or safety light curtain
monitoring with 3N/O safety circuit output and 1 N/C+ 4-solid-state signalling outputs for PLC, terminal block connection
integrated in module, supply voltage: 24VAC/DC.
 
XPSAF5130- Preventa Safety Module For Emergency stop and switch monitoring, with 3N/O safety circuit output,terminal
block connection integrated in module, supply voltage: 24VAC/DC.
 
Refer the attached file for technical catalogue of GSKC24VACDC, XPSAK311144 and XPSAF5130.
Was this helpful?
What can we do to improve the information ?