Technical FAQs

Ask a Question

What is function of Zelio module SR3XT43BD.

SR3XT43BD is a Zelio Logic Analogue Input/Output Extension module including maximum 2 Number of inputs 0-10V or
2 number of Inputs 0-20mA OR 1 number of Pt100 signal and maximum 2 numbers of Analogue outputs 0-10V.
The Analogue I/O extension module SR3XT43BD must be connected to an SR3   Zelio modular smart relay with 24VDC supply.
Was this helpful?
What can we do to improve the information ?