Technical FAQs

Ask a Question

What are default settings of the ELF-3200 series meter.

If there is no instruction from the customer while ordering, meter will be dispatched with the following default settings. 


Was this helpful?
What can we do to improve the information ?