Technical FAQs

Ask a Question

The DigitAN EM 6400 meter display went blank abruptly. What could be the reason and how to rectify it.

This may be due to over voltage/temperature.
 
DigitAN has inbuilt over voltage/temperature protection which will interrupt the functioning of the meter temporarily,
when the voltage/temperature rise beyond the specified limit, as a pre-cautionary measure.
 
To make the meter to function again, interrupt the power supply or reduce the voltage/temperature within the limit.
 
Still the problem persists call our customer care for further assistance.
Was this helpful?
What can we do to improve the information ?