Technical FAQs

Ask a Question

What is the maximum input counting frequency for TSX CTY 2C.

The maximum counting frequency for TSX CTY 2C is 1 MHz.
The range is from 125KHz to 1MHz
Was this helpful?
What can we do to improve the information ?