Technical FAQs

Ask a Question

What is the difference between 490 NAD 911 03 and 490 NAD 911 04 profibus connectors.

The 490 NAD 911 03 is end terminator connector and 490 NAD 911 04 is intermediate profibus connector on the bus.
Was this helpful?
What can we do to improve the information ?