Technical FAQs

Ask a Question

Which model of Connexium switches are supported as dual ring switches in Quantum Ethernet Remote IO Offer.

Below given are the switches which can be used
These switches have predefined configuration files that have been carefully engineered to provide service level guarantees
 that this solution offers towards Quantum Ethernet Remote IO offer.
Was this helpful?
What can we do to improve the information ?