Technical FAQs

Ask a Question

Can a rectangular sensor on the micro logic 7.0 be placed on the incoming side of the breaker than the outgoing without affecting their operation.

Yes, it is possible to install this rectangular sensor ( reference 33574 ) upstream if it is not possible to install it differently.
The earth leakage protection will work correctly without any restriction.
Was this helpful?
What can we do to improve the information ?