Technical FAQs

Ask a Question

What is the operation of dynamic braking on Altivar 71 drive with braking resistor.

For dynamic braking with braking resistor, the drive switches on the braking transistor when the value of bus voltage
is more than threshold voltage. If the value of the bus voltage is less at the same threshold, the transistor switch off
 
Refer to attached file for voltage value: The threshold is OBR.
Was this helpful?
What can we do to improve the information ?