Technical FAQs

Ask a Question

Is it possible to have a capacitor bank to correct the network power factor upstream of Altivar 71/61 drive.

It is not recommanded to use capacitor bank with ATV.So,normaly,it is not needed to correct the cos phi of the drive because,with a drive
the cos phi is closed to 1 (at full load) .
Was this helpful?
What can we do to improve the information ?