Technical FAQs

Ask a Question

Why there is an error “The Type Manager cannot find the type XXMIT” when I try to implement from Type Library Browser.

This error doesn’t mean that you have not installed FFB Library Properly. Your Library is installed properly that’s you are
able to see the XXMIT Function Block in Types Library Browser.This error generally occurs when you are using Quantum CPU
which is having the Software Version less than V2.30.
In order to use XXMIT Function Block, upgrade the CPU OS version to greater than V2.30.
Was this helpful?
What can we do to improve the information ?